How can we help you today?

Do the CT and PT need to be removed during the process of removing the Hardware Lock off the COM Card of the ION7650?

Issue

Do the CT and PT need to be removed during the process of removing the Hardware Lock off the COM Card of the ION7650?

Product Line

ION7650

Environment

ION7650 COM Card

Resolution

The following should be considered:
- The Meter must be powered off while performing the next step.
- CT and PT connections must be completely removed.