Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you power up the ATV32 with an external 24Vdc supply?

Issue:
ATV32 power up with an external 24Vdc supply

Product Line:
ATV32

Environment:
All serial numbers

Cause:
To maintain control power to the drive.

Resolution:
Yes, the P24 terminal and COM are the connections that can be used for external 24VDC.
**NOTE:  This does not apply to the ATV320, the P24 terminal on ATV320 is only used to supply the STO (Safe Torque Off) terminal, P24 will not accept 24v.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)