Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Configuring MBP_MSTR Function to Explicit Read Quantum PLC via Native Modbus Plus Port
This procedure has been created with Unity Pro v12 software. It will cover the configuration and setup for the MBP_MSTR function block performing an explicit read operation from a node on a Modbus Plus network through the native Modbus Plus port of a Quantum 140CPU65160 processor.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center