Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I install surge suppressors in the field for Trio and Accutech products? Does it go on the mast or can it be indoors, attached to the chassis, then GND?

The surge suppressor is not water tight, so it needs to be mounted inside a water-tight cabinet or building. The ground cable from the suppressor must be routed in such a manner as to keep the path to earth ground as short and straight as possible. The ground cable run must minimize sharp bends and must avoid metal conduit, which cause high impedance to the very high frequency energy surge. Bends in the ground cable must be as gentle as possible, and if conduit is required, the ground cable should be run through PVC conduit.

Schneider Electric Egypt and North East Africa