Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How Can to connect PT1000 probes to Zelio Temperature control relays ?

The Zelio Temperature control relays can not be connected with PT1000, hence we regret for unable to suggest a part reference form Zelio temperature control relay offer. If it is PT100, the customer can use REG24, REG48, REG96 series relays for temperature control application, hence kindly check the online selection tool's link below where you can choose the range then from the left hand side filter as per the specifications till reaching a specific reference that suits your requirements & applications:
https://www.se.com/ww/en/product-range/528-zelio-control/166478139-solution?parent-category-id=2800&N=1599450402&Nrpp=10&filter=business-1-industrial-automation-and-control#tabs

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: