This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Actually Atex pushbuttons like XB4...EX are an ATEX certified product, the certification is done for the whole product (i.e. the complete unit including the contacts)
According to ATEX directive, the complete product has to be certified & tested according to special rules & then it is marked if it complies to ATEX standards
Actually, we do not have special reference for ATEX pushbuttons contacts as spare part (i.e. no ATEX marking special for the contacts), However, For ATEX, XB4 or XAW products, the contact block is the same as in standard one of XB4 (ZBE10*), only the head that is marked ATEX
So, if the customer requirement is to replace ZBE10* contact block in an existing XB4..EX with a new one (exactly same contact as the initial one existing), then this solution is valid
But if the customer request is to add additional contact ZBE10* to XB4..EX pushbutton, then this is not an ATEX certified solution as it is not tested
According to ATEX directive, the complete product has to be certified & tested according to special rules & then it is marked if it complies to ATEX standards
Actually, we do not have special reference for ATEX pushbuttons contacts as spare part (i.e. no ATEX marking special for the contacts), However, For ATEX, XB4 or XAW products, the contact block is the same as in standard one of XB4 (ZBE10*), only the head that is marked ATEX
So, if the customer requirement is to replace ZBE10* contact block in an existing XB4..EX with a new one (exactly same contact as the initial one existing), then this solution is valid
But if the customer request is to add additional contact ZBE10* to XB4..EX pushbutton, then this is not an ATEX certified solution as it is not tested
Released for: Schneider Electric Egypt and North East Africa