Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Conditional rated short circuit current (Inc/I∆c) , For RCCB-ID B type ?
The Conditional rated short circuit current :
25/40 A with FU 80 A gG fuse  ==>  10,000 A
63 A with FU 100 A gG fuse   ==>  10,000 A
80/125 A with FU 125 A gG fuse ==>  10,000 A