Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an InFb or internal error 11 on the ATV630 and ATV930 Process drives?
Issue:
ATV660- What can cause a internal error 11 (InFb)?

Product Line:
ATV630, ATV930, ATV660 and ATV960

Environment:
All

Cause:
-Loose connection of the temp. sensors.
-Not correctly connected plugs
- Calibration data of the thermal sensors not correct.

Resolution:
All internal temperature sensor is monitored, for short circuit or open circuit.
If a short circuit / open circuit is detected the InFb occurs.