How can we help you today?

What’s the maximum number of words for data in flow variables in BMENOP0300 module?

Question: What’s the maximum number of words for data in flow variables in BMENOP0300 module?
Answer: 4000 words. The maximum number of input words includes the sum of client and server input words. The maximum number of variables depends on the data types included in the application because the lengths of different data types varies. Module memory contains the most current (real-time) value for data in flow.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center