Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the switchgear control failure codes in Easergy T300?

Whenever a command is issued a code appears in the event log for each control operation. These are the following codes and the reasons indicating the status of each control operation.

Main switchgear control failure variable
Value (potential issue code) Description
0Command completed successfully
1Local command blocked because switch position is intermediate or unknown
2Local command blocked because switch position is already in correct state
3Local command canceled by user
4Switch position did not change within configured maximum operation time
5Command blocked by Head Unit interlocks, e.g. potential motor supply issue or battery low
6Command did not execute due to timeout waiting for enable from Head Unit
7Local command blocked because disabled by configuration
8Local command blocked because local/remote status is unknown
9Local command blocked because local/remote status is remote
10Local command blocked because automation is on
11Remote command blocked because automation is on
12Sectionalizer command blocked because automation is off
13Sectionalizer command blocked because local/remote status is unknown
14Sectionalizer command blocked because local/remote status is local
15Unexpected command source (firmware potential issue)
16Remote command blocked because requested position is not a valid value
17Command blocked because a command is already in progress for this module
18Command blocked because the power shutdown signal is active
19Command blocked because a command is already in progress for another module
20Command blocked because measured switch position is intermediate or unknown
21Command blocked because measured switch position is the same as the requested position
22Command blocked because ground (earth) switch position is not open
23Open command blocked because external input is false
24Open command blocked because external input is true
25Close command blocked because external input is false
26Close command blocked because external input is true
27Commands blocked because module behaviour mode is off
28Command blocked because switch controller is in local mode
29Command blocked because switch controller local/remote input is undefined
30Command blocked because protection trip lockout is active
31Command blocked because the OPEN/CLOSE command is in progress
32Command blocked because a self-test is in progress

Schneider Electric Egypt and North East Africa

Attachment(s)
What are the switchgear control failure codes.pdf [236.22 KB]