Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to start with a very first new Safety M580 CPU into a Safety configuration ?
When RIO is in the configuration and before to start a new configuration, user has to :
1/ Set the date and time into the PLC , CPU out of the final destinated rack ,
2/ Set an NTP server into the configuration (either external server or CPU as NTP server),
3/ Place CPU into the rack to be used and start the configuration,
4/ Make sure all configured safety I/O modules are unlocked ( eventually, use the top blue button to unlock the locked module )


Reminder : it is required to set the date and time into the PLC in order to have a reliable safe communication between CPU and safety IOs module.

If the configuration with Safety I/Os have been started before the configuration of the time into the CPU,  a synchronization of the time between IOs and CPU is necessary either by :

  • 1: forcing the time using %SW128 see the FA333333 how to proceed
  • 2: downloading again the application into the PLC
  • 3 : doing a power cycle of the entire configuration (CPU AND IOs safety modules)

Schneider Electric Egypt and North East Africa

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category: