Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use the same device for either feeder or motor protection?
Yes, by selecting the “Application mode” either to “Motor” or “Feeder” mode. This is possible for the Easergy P3U standard devices.