Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I define Trip Circuit Supervision?
Trip Circuit Supervision require a logic function to be created. In this example covering TCS with 2 inputs DI1 and DI2 is used for breaker open and close status. The inputs must be inverted (below NC selection). Please refer to manual for connections. For e.g. Easergy P3 standard, refer to chapter 6.16

Schneider Electric Egypt and North East Africa

Attachment(s)
TCS.JPG.jpg [19.28 KB]