Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why would the ATV320 drive in the RDY state, not allow programming changes?

Resolution:
Verify Function block is disabled.   ATV32 / 320 – Disable Function Blocks - To turn off the function blocks

Go to the FULL menu enter  Fbn enter > FbCd enter and set this to STOP

Now you can adjust parameters or go back to the factory settings   ConF > FCS > FCS1 = InI, FrY – InI, GFS – YES (2s) (all 3 in this order)

** Keep in mind that a factory reset will remove the Function Block program and the application will no longer work as it previously did

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)