Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to disable the On Screen Keyboard for the HMIG5U/HMIG5U2?
Issue:
Looking for a way to hide the On Screen Keyboard for the HMIG5U/HMIG5U2.

Product Line:
Magelis iPC, Magelis HMIG5U, Magelis HMIG5U2

Resolution:
To disable the On-Screen Keyboard that is hidden in the top left corner of the HMIG5U/HMIG5U2, you will need to do the following:

1) Open the Control Panel
2) Search for "Tablet PC Settings"
3) Click on the "Other" Tab
4) Press the link "Go to Input Panel Settings"
5) Find the check box "Use the Input Panel tab" and uncheck it.
6) Press Apply and then OK