Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an ATV212 logic input be programmed as both a run command and a preset speed?
Issue:
ATV212 run activate and preset speed on the same input.

Product Line:
S-Flex ATV212

Environment:
All

Cause:
Set up Run and Preset speed at the same time.

Resolution:
Yes.  The logic inputs have options for combination assignments.

22 = run forward + preset speed 1
23 = run reverse + preset speed 1

Eg:  Logic input F assignment F111 = 22
Input OFF - Motor stops
Input ON - Motor runs forward at speed set by Sr1 (preset speed 1)