Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Common mode filter for bearing current reductions for the ATV600 and ATV900 drives frame size five drives?
Issue:
Common mode filter for bearing current reductions for the ATV600 and ATV900 drives

Product Line:
ATV600 and ATV900 drives frame size 6

Environment:
All

Cause:
Filter for bearing current reductions

Resolution:
The part number is VW3A5505 and its value of inductance is 183.2 uH

Schneider Electric Egypt and North East Africa

Attachment(s)
Altivar Process ATV900_VW3A5505.pdf [91.49 KB]