Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I split bits from a word to digital points?

DISCLAIMER

The example below is intended to demonstrate one or more features or methods and is presented as a configuration example only. Schneider Electric assumes no liability for the use or application of this example or any portion thereof.



Sometimes it is necessary to extract the bits from a word and split those to individual digital points. One way of doing this is by a logic program.
In this example, we will use a structured text library containing a function (Word2Bits) that uses "AND" operators to extract the bits from a word (16 bits). The structured text library is attached to this article and we will show how to import and use it in a function block diagram (FBD) logic program in ClearSCADA.

After we download the attached .ZIP file and extract "Structured Text Library containing the Word_2_Bits function example.SDE", we can import the .SDE to ClearSCADA 2015 R1 or newer. On the following screen capture, we imported the .SDE file to a folder called "Example":

Library

As you can see, the input is an unsigned integer and the outputs will be booleans. Feel free to check the code in ViewX.

In order to use the function, we will create a FBD logic program and link the library to it:

Select Library

Now we have the function available for use (right-clicking on the programming area):
Insert block
Function block
Now we can link the input and outputs as required.

Schneider Electric Egypt and North East Africa

Attachment(s)
Structured Text Library containing the Word_2_Bits function example.zip [117.36 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: