How to configure the BMXNOM200 for 'Stop on Reception' using both CR and LF
Issue
How to configure the BMXNOM200 for 'Stop on Reception' using both CR and LF
Product Line
BMXNOM0200
Environment
Unity, Windows 10
Resolution
To configure the NOM serial port for the Stop on recption using both CR and LF, reference the example in the following screen capture.
How to configure the BMXNOM200 for 'Stop on Reception' using both CR and LF
Product Line
BMXNOM0200
Environment
Unity, Windows 10
Resolution
To configure the NOM serial port for the Stop on recption using both CR and LF, reference the example in the following screen capture.
Released for: Schneider Electric Egypt and North East Africa