Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In which material is made the ZBYD06*** ?
The base material is plastic (ABS), front is silver anodized, backside self adhesive.