Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the din rail mounting kit part number for the ATV320?

Article available in these languages: Japanese

Issue:
Is there din rail mounting kit available for the ATV320 drive?

Product Line:
ATV320

Environment:
All

Cause:
Desire to utilize din mounting kit option

Resolution:
The mounting kit part numbers for this drive are VW3A9804 or VW3A9805.

VW3A9804 covers the following range of drives:
ATV320U02M2C
ATV320U04M2C
ATV320U06M2C
ATV320U07M2C
ATV320U02M3C
ATV320U04M3C
ATV320U06M3C
ATV320U07M3C

VW3A9805 covers the following range of drives:
ATV320U11M2C
ATV320U15M2C
ATV320U22M2C
ATV320U11M3C
ATV320U15M3C
ATV320U22M3C
ATV302U04N4C
ATV320U06N4C
ATV320U07N4C
ATV320U11N4C
ATV320U15N4C
ATV320U07S6C
ATV320U15S6C

Note: The din rail mounting kits are only available for the above drives. The other drives not list above do not have a din rail kit.