Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does an ATV320 low speed setting, LSP, only go up to 50Hz?

Issue:
ATV320 LSP is restricted to 50Hz maximum

Product line:
ATV320, Altivar 320

Environment:
n/a

Cause:
Basic settings

Resolution:
The LSP (Low Speed) can only be adjusted to TFR (Max Frequency), but also restricted to the HSP (High Speed) setting.
First check that BFR (Standard Mot freq) is set to 60 (60Hz NEMA).
Next check the setting of TFR (Max frequency).  Factory setting is 60Hz but goes to 72Hz when BFR is adjusted to 60Hz.
Last check the HSP (High Speed) setting.

Once TFR and HSP are at 60Hz, or higher, the LSP can be adjusted above 50Hz

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Schneider Electric Egypt and North East Africa