Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What terminal blocks can be used with a BMXDDI1602 I/O module?

Issue:

What terminal blocks can be used with a BMXDDI1602 I/O module?

Product Line:

BMXDDI1602

Resolution:

BMXDDI1602 I/O module can be used with one of the following terminal blocks:

- BMXFTB2000 - Cage clamp
- BMXFTB2010 - Screw clamp
- BMXFTB2020 - Spring clamp

The terminal blocks will have to be ordered separately, the BMXDDI1602 I/O module does not come with any terminal block.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)