Issue:
What terminal blocks can be used with a BMXDDO1602 I/O module?
Product Line:
BMXDDO1602
Resolution:
BMXDDO1602 I/O module can be used with one of the following terminal blocks:
- BMXFTB2000 - Cage clamp
- BMXFTB2010 - Screw clamp
- BMXFTB2020 - Spring clamp
The terminal blocks will have to be ordered separately, the BMXDDO1602 I/O module does not come with any terminal block.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: