Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a parameter in the ATV212 that will change the output phase rotation/direction of the motor?
Issue:
ATV212 phase rotation swap parameter

Product Line:
ATV212/ATV21

Environment:
All

Cause:
Output phase rotation

Resolution:
No. To change the output phase rotation on the ATV21 / ATV212, you must swap 2 of the motor leads.