Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How does one program the ATV212 Drive so that RY relay will trigger when a speed threshold is reached?
Issue:
ATV212 configuration so that RY relay will trigger when a speed threshold is reached

Product Line:
Altivar 212

Environment:
All

Cause:
Frequency reference reached

Resolution:
Using RY relay for speed reached functionality.
F130 from the factory is already programmed as 4 for speed reached.
F100 can be programmed to value desired in hz.

The RY relay will actuate when the VFD output frequency is greater than or equal to the F100 setting.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: