Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What power quality measurements are available in PM1130H meter ?

Issue

What power quality measurements are available in the PM1130H meter?

Product Line

PowerLogic PM1000 Series (PM1130H)

Environment

PM1130H Energy Meter – Power Quality Measurement Capabilities

Resolution

The PM1130H meter provides complete harmonic distortion metering, recording, and real-time reporting, up to the 15th harmonic for all voltage and current inputs (depending on the selected wiring configuration).

The following power quality measurements are available in the meter:

  • Total Harmonic Distortion (THD%) for current and voltage
    • Displays line-to-line or line-to-neutral values, based on the selected wiring configuration.