Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV320 - Why don't I see nPr [nominal motor power] in the SIn [Simply Start] menu?
Issue:
Unable to see nPr in the SIn menu on the Altivar Process ATV630

Product Line:
ATV630

Environment:
All

Cause:
Programming

Resolution:
This occurs when CONF > FULL > DRC- > ASY –
  • nPC is set to CoS
(Note: For the majority of applications, CoS seems to work better)

**When the ATV320 replaces ATV312, the correct setting is CoS**

Schneider Electric Egypt and North East Africa

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Category: