Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which types and sizes of wires can be connected to the PRA90047 terminal?
In the PRA90047 it is possible to mount the following wires:
- from 0.5mm2 to 4mm2 - solid, flexible or flexible with ferrule.
- from 0.5mm2 to 6mm2 - solid or flexible (without ferrule).