{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
M241/258 Frequency meter output is not 0 when no pulses are received
M241 and M258 frequency meters have a "Validity" output which is FALSE when no pulses are received after the duration defined in "Time base" parameter ( 10, 100 or 1000 ms).

When "Validity" output is FALSE, "CurrentValue" has the last computed frequency value (not 0), but this value must be ignored.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: