Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use Lexium 05 for BMH motors?
No. It is not possible to drive BMH from LXM05. The LXM05 needs a temperature sensor and the BMH has no sensor.
LXM05 cannot drive BMH. Only BRH, USH, BSH and SER can be driven by LXM05.