How can we help you today?

EcoStruxure Hybrid DCS [4.3 SP1]: Cannot login in FlexNet License Administrator of Floating License Manager v2.1.0.0

From Floating License Manager (FLM) v2.1.0.0, the default "admin" user has been withdrawn.To login in the "Administration" section, you will have to enter the Windows User used to install the FLM, in the format of:
Domainname\Username or Computername\Username.

If you don't remember who has installed the Schneider Electric Floating License Manager, you need to reinstall it to add again a new default user account.

For further information, see the attached FLM v2.1.0.0 release notes.

Schneider Electric Egypt and North East Africa

Attachment(s)
FLM_ReleaseNotes.EN.rtf [17.46 KB]