Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How does PM5500 series meter calculates TDD (Total Demand Distortion)

Issue

Is there a more detailed description of how the PM5000 series meter calculates TDD (Total Demand Distortion

Product Line
PM5500 series

Environment
Documentation

Resolution

  • Total demand distortion (TDD) is the per-phase harmonic current distortion against the full load demand of the electrical system
  • TDD indicates the impact of harmonic distortion in the system
  • For example, if your system is showing high THD values but a low demand, the impact of harmonic distortion on your system might be insignificant
  • However at full load, the THD value for the current harmonics is equal to TDD, so this could negatively impact your system
  • TDD (total demand distortion) evaluates the harmonic currents between an end user and a power source
  • The harmonic values are based on a point of common coupling (PCC), which is a common point where each user receives power from the power source
  • The meter uses the following equation to calculate TDD:
TDD formula
  • Where ILoad is equal to the maximum demand load on the power system and HC is Harmonics Count
  • Harmonic content (HC) is equal to the RMS value of all the non-fundamental harmonic components in one phase of the power system.
  • The meter uses the following equation to calculate HC:
HC (Harmonic Content) formula

Schneider Electric Egypt and North East Africa

Attachment(s)
PM5500_User_Guide.pdf [3 MB]