Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The varplus logic displays "SPL/Nr ALARM".What action to be taken?
This alarm indicates that the current step size is less than 75 % of the initial size. It is recommended to replace the capacitor.