How can we help you today?

Importing a '.cid' file for the IED server returns 'Operation error'.


Issue
Importing a '.cid' file for the IED server returns the error 'Operation error. The edition of selected SCL file doesn't match the module setting'.

Product Line
BMENOP0300

Environment
Unity, Windows 10


Resolution
Importing a '.cid' file for an IED server configuration returns the error 'Operation error. The edition of selected SCL file doesn't match the module setting.

fghj

This will occur if the user tries to import a '.cid' file that is defined for an IEC client.