Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a replacement for the HMIGXU5512 series?

Issue:
Is there a replacement for the HMIGXU5512 series?

Product Line:
HMIGXU series

Resolution:
The HMIGXU5512 (HMIGXU series) is an HMI sold solely in the China Market. There is no North American equivalent as the screen resolution is 800 x 480. Customers are instructed to contact their original Machine builder to have them send a replacement.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)