Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the PM5560 series meter Measurement Canada Approved
Issue
Is the PM5560 series meter Measurement Canada Approved?

Product Line
PM5500 series meter

Environment
PM5500 series meter

Cause
Need a PM5500 series meter that is approved by Measurement Canada for Revenue Billing applications.

Resolution

We have two RMICAN references for the PM55xx family
METSEPM5562PM55xx, RMICAN approved, HW lockable
METSEPM5562MCPM55xx, RMICAN approved, Factory sealed

The PM5562 meter has been tested and is approved by Measurement Canada for Revenue Billing applications. The customer would be responsible for having the meter sealed at a qualified sealing shop such as Fortis.

The PM5562MC version is approved by Measurement Canada and is sealed by a sealing shop such as Fortis prior to being shipped to the end customer.