Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you order the ATS22 soft starter with a specific firmware version?

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

Issue:
ATS22 soft starter with a specific firmware version order.

Product Line:
ATS22

Environment:
All

Cause:
Wants a specific firmware version.

Resolution:
The firmware update is done on the mfg side not the end customer side. In most cases the end customer will not need to update the firmware because their soft starter works with the previous version no problem. But if they buy a new product it will most likely include the updated firmware.