Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many SCADA clients can be connected to an Easergy T300 using IEC 104 protocol?
  • There is a limitation of 8 redundant connections to create multiple SCADA channels using the IEC104 protocol. Create 1 channel per client.
  • Make sure to fill-in the Remote IP@ list field. It shall be different for every channel
  • Please refer to attached file

Schneider Electric Egypt and North East Africa

Attachment(s)
How many SCADA clients can be connected to an Easergy T300 using IEC 104 protocol.pdf [313.34 KB]