Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is the JOG function programmed on the ATV340 drive?
Issue:
How to program the ATV340 drive for JOG?

Product Line:
Altivar 340

Environment:
All

Cause:
N/A

Resolution:
From the main menu, select menus Complete settings -> Generic functions -> Jog.
Default settings as follows.
JOG    Jog assignment, set as appropriate
JGF    Jog frequency,    10 Hz.
JGT    Jog delay,    0.5 s.

See attached file.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV340 JOG.pdf [135.48 KB]