Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ION meter template file be read before sending it to the meter?

Issue
A user wants to view an ION template file before sending it to the meter

Product Line
Powerlogic ION meters

Environment
ION Setup
Text Editor

Resolution

The meter template file (DCF) is not human-readable and therefore cannot be read before sending it to the meter. When opened in a text editor like notepad, the file will display non standard characters.