Is the BMENOC0301 module hot swappable?
Issue
Desire to replace the NOC without impacting the CPU.
Product line
Modicon M580
Resolution
The BMENOC0301 module can be replaced simply by removing the cables, lifting it out of the backplane then dropping the new one in and replacing the cables. It will receive the configuration from the M580 after booting up.
Your network will now include an Ip address that has changed its MAC address. This may or may not raise a flag depending on your specific installation.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.