Why I cannot any more write the TRUE-VALUE field for BMXSRA0405 and BMXSDO0802 modules?
In a project created with Unity Pro V13.0, the TRUE-VALUE field for BMXSRA0405 or BMXSDO0802 modules is in Read/Write. With Unity Pro V13.1, the TRUE-VALUE field is now Read Only, in compliance with documentation for BMXSRA0405 or BMXSDO0802 modules.
For a project that has been created with Unity Pro V13.0, the TRUE-VALUE field will remain Read/Write when the project is opened in STA (or STU) format. It will only be Read Only for a new Unity Pro V13.1 project, or if a project is imported from ZEF format
For a project that has been created with Unity Pro V13.0, the TRUE-VALUE field will remain Read/Write when the project is opened in STA (or STU) format. It will only be Read Only for a new Unity Pro V13.1 project, or if a project is imported from ZEF format
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.