Issue:
Does the Process Drives have Torque Limitation and do you have to assign an input?
Product Line:
ATV900
Environment:
All
Cause:
Wiring
Resolution:
The ATV900 series drives do have the Torque Limitation feature. It is found in Complete Settings > Generic Functions > Torque Limitation and can either be set to YES for always active or assigned to a digital input for activation.
Does the Process Drives have Torque Limitation and do you have to assign an input?
Product Line:
ATV900
Environment:
All
Cause:
Wiring
Resolution:
The ATV900 series drives do have the Torque Limitation feature. It is found in Complete Settings > Generic Functions > Torque Limitation and can either be set to YES for always active or assigned to a digital input for activation.
Released for:Schneider Electric Egypt and North East Africa