Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can you confirm whether SEPAM 80 will support for IEC 61850 Edition 1 & Edition 2

Description:
Whether SEPAM 80 will support for IEC 61850 Edition 1 & Edition  2?

Product family:
SEPAM 80

Resolution:
Yes , SEPAM 80 will support for IEC 61850 Edition 1 & Edition  2.

However, thanks to verify with the selected model as per the order code with your local pre sales/PAE/FO team.