Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How do I use UMAC V2.2 to convert a Unity Quantum application to an M580 application?

Issue:
Converting a Unity Quantum application to an M580 application using the UMAC v2.2 tool

Product Line:
Quantum, Unity Pro, M580, 1MMCSVCZMSXAZZ,

Resolution:
In order to use the the UMAC conversion utility to migrate a Unity quantum application to M580, the user must meet the following criteria.

Prerequisites:
1: The user must have Unity Pro XL =>V12.0 installed on his PC
2: UMAC V2.2 will only accept a Quantum ZEF file created in Unity Pro XL => V12.0
3: Install UMAC and select upgrade to "Standard" mode.

Conversion process
1: Launch the UMAC converter using the "Run as Administrator" option.
2: When prompted, point to the Quantum ZEF file you wish to convert to M580
3: Execute the conversion when prompted by UMAC.
4: Save the converted ZEF file.
5: Generate conversion report from within UMAC.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)