How can we help you today?

PlantStruxure PES [V3.1 -> V4.3] & EcoStruxure Hybrid DCS [2018]: embedded Versions

Goals and Symptoms


Provide list of participants versions delivered per release

Facts and Changes

Release VersionOperating system of the workstation
PES Server/Eng client/Operation server & client
Operating system of
the virtual machine
Unity ProVijeo CitectOFSDate of delivery
PES V3.1Windows 7 Pro (x32 & x64)Windows 7 ProV7.0V7.30V3.40June 2013
PES V3.1 SP1Windows 7 Pro (x32 & x64)Windows 7 ProV7.0V7.30V3.40 SP4October 2013
PES V4.0Windows Server 2012,  Windows 7, 8.1 Pro (x32 & x64)Windows 7 ProV8.1V7.40 SP1V3.5 SP3January 2015
PES V4.0 SP1Windows Server 2012,  Windows 7, 8.1 Pro (x32 & x64)Windows 7 ProV8.1V7.40 SP1V3.5 SP3September 2015
PES V4.1Windows Server 2012,  Windows 7, 8.1 Pro (x32 & x64)Windows 7 ProV10V7.40 SP1V3.5 SP3February 2016
PES V4.2Windows Server 2012,  Windows 7, 8.1 Pro (x64)
Operation client: Windows 7, 8.1 Pro (x32)
Windows 7 ProV11.0 + HF1, HF PES_adaptation2015/V7.50 SP1 V3.5 SP8June 2016
PES V4.2 SP1Windows Server 2012,  Windows 7, 8.1 Pro (x64)
Operation client: Windows 7, 8.1 Pro (x32)
Windows 7 ProV11.0 + HF1, HF PES_adaptation2015/V7.50 SP1 V3.5 SP8November 2016
PES V4.2 SP2Windows Server 2012,  Windows 7, 8.1 Pro (x64)
Operation client: Windows 7, 8.1 Pro (x32)
Windows 7 ProV11.0 + HF1, HF PES_adaptation2015/V7.50 SP1 V3.5 SP8January 2017
PES V4.2 SP3Windows Server 2012,  Windows 7, 8.1 Pro (x64)
Operation client: Windows 7, 8.1 Pro (x32)
Windows 7 ProV11.0 + HF1, HF PES_adaptation2015/V7.50 SP1 V3.5 SP8April 2017
PES V4.3Windows Server 2012,  Windows 7, 8.1 Pro (x64)
Operation client: Windows 7, 8.1 Pro (x32)
Windows 7 ProV11.0 + HF1, HF PES_adaptation (Simulator V11)2015/V7.50 SP1 + Patch11V3.60 SP3June 2017
PES V4.3 SP1Windows Server 2012,  Windows 7, 8.1 Pro (x64)
Operation client: Windows 7, 8.1 Pro (x32)
Windows 7 ProV11.0 + HF1, HF PES_adaptation (Simulator V11)2015/V7.50 SP1 + Patch11V3.60 SP3November 2017
Hybrid DCS 2018Windows Server 2012,  Windows 7, 8.1, 10 Pro (x64)Windows 10 ProV13Citect 2016V3.60July 2018