Issue
User would like to know the differences between the Digital Output Behaviour Modes "Normal", "Timed", and "Trip Coil"
Product Line
PM5300
PM5500
Environment
Front panel or ION Setup
Resolution
Descriptions of the three (3) digital output behaviour modes are below.
Normal:
User would like to know the differences between the Digital Output Behaviour Modes "Normal", "Timed", and "Trip Coil"
Product Line
PM5300
PM5500
Environment
Front panel or ION Setup
Resolution
Descriptions of the three (3) digital output behaviour modes are below.
Normal:
- Digital output will turn ON when the specified external or alarm condition is met as defined in Control Mode
- The digital output remains ON only while the alarm is active
- Digital output will turn ON when the specified external, demand sync, alarm, or energy condition is met as defined in Control Mode
- The digital output remains ON for the time period (in seconds) defined in the "On Time" setup parameter
- Digital output will turn ON when the specified external or alarm condition is met as defined in Control Mode
- The digital output remains ON until the command number 6004 is sent to the meter from a PLC or PC.
- Please check the command structure in the Modbus register list at PowerLogic PM5000 Series (PM5100, PM5300, PM5500) Modbus Register List
Released for: Schneider Electric Egypt and North East Africa