How can we help you today?

OFS server version 3.61 shuts down after starting.

Issue
OFS server shuts down a few seconds after it starts.

Product Line
OFS version 3.61

Environment
Windows 10

Resolution
​The OFS server shuts down a few seconds after it starts.

The reason why this occurs is due to OFS not being able to find the Temp folder.  OFS needs to create a folder in the 'C:\Temp' folder.
If it cannot find the Temp folder, it will shut down.

To resolve the issue, create a 'Temp' folder in the 'C' drive of the PC..

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center