Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you run a motor with the ATV320 to drive up above 60 hz?

Issue:
How to allow the ATV320 to drive up above 60 hz?

Product Line:
Altivar 320

Environment:
All

Cause:
N/A

Resolution:
Go into CONF, FULL, SIM-, and set TFR (max frequency) to a value above 60 hz.
Next set HSP (high speed) under SIM- menu to value desired to a max value of TFR.
HSP -High speed can not be set higher than tFr -max frequency.